LabVIEW example application EtherNet TCP/IP (REST) Using the REST protocol, the new generation of controllers / drives can communicate with LabVIEW via the Ethernet interface. More details
Example Applications: Siemens S7–1500 Modbus TCP Our example application shows how Nanotec’s motor controllers/drives and integrated motors can be controlled via Siemens S7. More details
Example Program Rockwell Add-Ons Following this example, you can quickly set up our controllers / drives via EtherNet/IP using a CompactLogix or ControlLogix PLC and Rockwell's Studio 5000. Rockwell and EtherNet/IP… More details
LabVIEW Example Application USB/VCP By using our VCP driver (Virtual ComPort), our new generation of controllers can also communicate with LabVIEW via the USB interface. More details
Parameterization of TwinCAT2/CANopen Setting up TwinCAT to operate CANopen devices as NC axis and in Cyclic Synchronous Position (CSP) Mode. More details
Example Programs OMRON NX1P2 You can use these examples and the Application Note to quickly set up our controllers with an OMRON PLC via EtherCAT. More details
Parameterization of TwinCAT3/EtherCAT Configuration of TwinCAT3 to operate Nanotec controllers via EtherCAT as a box or NC axis in position or cyclic synchronous position (CSP) mode. More details
Example Programs IDEC You can use these examples and the Application Note to quickly set up our controllers with an IDEC-PLC via Modbus TCP. More details
Example Programs Trio MC4N-ECAT Based on the examples and the application note, you can quickly commission our controllers via EtherCAT with a Trio PLC. More details