Example Programs IDEC

You can use these examples and the Application Note to quickly set up our controllers with an IDEC-PLC via Modbus TCP.

This example shows the principle of using Plug & Drive interface in a WindLDR ladder diagram.
13 KB
This example shows how the position mode can be used in a WindLDR ladder diagram.
14 KB
Starting up a Nanotec Controller/Drive with IDEC SmartAXIS FT1A-H40RSA
Version 1.0.0
1 MB
Indietro

Domande? Commenti?

Avete domande o commenti su questo articolo?

Contatta l'assistenza